IMXRT1176 BUS FAULT: IMPRECISERR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXRT1176 BUS FAULT: IMPRECISERR

793 次查看
Gokberk
Contributor I

Hi,

There is a 16 Mb external flash on our custom board. I can easily debug the processor with McuXpresso IDE. I can also write and read with the Secure Provisioning tool. Then we started using 64 Mb flash instead of 16 Mb flash. When I debug through the IDE, an error occurs before reaching the main() function, as shown in the image below. When I examine the Memory, I see it is writing correctly to the flash, but I guess it cannot boot. It cannot run the code when I write it directly to 64 Mb flash with the Secure Provisioning Tool. Thanks for your help.

error.png

0 项奖励
回复
1 回复

708 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Gokberk,

Are you still having issues debugging your custom board? If so, please let us know if there have been additional findings in this regard.

Regards,
Gustavo

0 项奖励
回复