IMXRT1172 flashloader not starting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1172 flashloader not starting

Jump to solution
3,191 Views
Kaidou
Contributor II

Hello.

I'm working with a IMXRT1172 board. I enabled the Encrypted (OTFAD) authenticated secure boot and enabled the HAB and I was able to flash the board.

Then yesterday i tried again to flash a new image and now the flashloader is not starting.

I get the following error:


### Load FlashLoader ###
blhost -t 5000 -u 0x1FC9,0x013D -j -- load-image "..\secure_provisioning0\bootable_images\signed_MIMXRT1172_flashloader.bin"
{
"command": "load-image",
"response": [],
"status": {
"description": "0 (0x0) Success.",
"value": 0
}
}
blhost succeeded
### Waiting FlashLoader to be initialized for 5 seconds ###
### Timeout wait value can be adjusted from Preferences ###
### Check presence of FlashLoader ###
blhost -t 2000 -u 0x15A2,0x0073 -j -- get-property 7 0
ERROR:SPSDK: Selected 'usb' device not found.
blhost failed

 

The board is correctly connected and in serial downloader mode.
I tried with another board with secure boot not enabled and the connection works.

What might be the issue?

Thanks

Tags (3)
0 Kudos
Reply
1 Solution
2,958 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

If you selected the HAB closed life cycle there is no way to disable HAB or change keys, since they are already burned. 

 

View solution in original post

0 Kudos
Reply
5 Replies
3,032 Views
Kaidou
Contributor II

Is it possible that the flashloader is signed with a different key than the SRK burnt into the board?

 

0 Kudos
Reply
3,003 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

Per my understanding , when HAB is enabled, the flashloader must be signed with keys derived from the same CA that was used to sign the image.

Are you still using the same workspace and keys ? Do you have the same certificate?

Best regards, 

Diego

 

 

 

 

0 Kudos
Reply
2,988 Views
Kaidou
Contributor II

Thanks for your reply!

I'm guessing I don't have the correct keys anymore. Is there a way to recover the board somehow?
But I don't have much hope.

0 Kudos
Reply
2,959 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Kaidou 

If you selected the HAB closed life cycle there is no way to disable HAB or change keys, since they are already burned. 

 

0 Kudos
Reply
2,929 Views
Kaidou
Contributor II

Ok!

Thank you very much for your help!

0 Kudos
Reply