IMXRT1170 EVK wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1170 EVK wake up

296 Views
ujwal_kumar_N_L
Contributor III

Hi community ,
Im currently working with the IMXRT1170EVK ,the board has gone to sleep now im unable to wake it up.
How do i flash some other program into the Flash .
Is there a way to use Secure provision and flash an image into the EVK .

PROBLEM .
1)The board has gone to sleep unable to wake up (Wake up pin has been changed ,no other means to wake up).
2) Need to use the EVK ,how to make sure its in default condition .
3)Steps to Flash the code or  steps to use Secure provision to achieve the above task .
Details :

Board :MIMXRT1170-EVK

Thank you and regards 
UJWAL 

0 Kudos
Reply
1 Reply

258 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for contacting NXP support.

I understand the concern can you please help me with some extra details in order to find a solution to your case:

  1. Are you using an SDK example and modify this?
    1. What SDK version are you using?
  2. You mentioned in the point one that the wake up pin has been changes (did you performed this change) .

Please help me with this point in order to proportionate a solution.

0 Kudos
Reply