IMXRT10xx Pad Control Register (more info?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT10xx Pad Control Register (more info?)

1,708 Views
bw1
Contributor IV

Is there some  AppNote, webinar, or similar which covers the details of the software pad control registers in more depth than the Reference Manual?   i.e. IOMUXC_SW_PAD_CTL_PAD_    If so please provide a link or some other location information for it? Thanks. 

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

1,625 Views
bw1
Contributor IV

This is the best thing I have found, see AN5078 attached. 

0 Kudos
Reply

1,625 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Brad,

Unfortunately, there aren't any application notes or webinars like the one you are looking for. The best option you have is to download the SDK for your evaluation board and use the examples along with the reference manual to understand how the software control registers works.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply