IMXRT106x bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT106x bootloader

Jump to solution
1,484 Views
markomarusic25
Contributor II

Dear sirs,

I read an paragraph in processor reference manual which says:

"The ROM bootloader provides an API for the user application to boot from a new updated application safely after In-Application Programming (IAP) or re-enter serial downloader mode for image update. See more details in the next section."

Then, it is explained how to send ROM into boot mode using API: "runBootloader (&arg);"

One part of the "arg" is boot image selection (0, 1, 2 or 3). Can someone please explain to me what does this image selection refer to? Is there a way to store 4 different images to flash memory, and this is the way to tell ROM which one of them to boot after reset? If yes, where can I find information about this feature?

Than you,

Marko

Labels (2)
1 Solution
1,245 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One may refer to the thread https://community.nxp.com/message/1189574 

Best regards

View solution in original post

1 Reply
1,246 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One may refer to the thread https://community.nxp.com/message/1189574 

Best regards