IMXRT1064 Unable to connect wire for probe index 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1064 Unable to connect wire for probe index 1

2,744 Views
Vinay3
Contributor I

Hi,

We are not able to connect in debug mode 

we are using MCUXpresso IDE v11.3.1_5262

MCUXpresso linkserver CMSIS DAP probes

Please find the attached images as reference for the error

 

Screenshot (1).png

Screenshot (5).png

 Kindly provide your support to resolve this issue.

regards,

Vinay

0 Kudos
Reply
7 Replies

2,735 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I'd like to confirm the below inquires with you.
1) Do you use the MIMIXRT1064 board for testing?
2) Does the error happen before or the first time arises?
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,715 Views
Vinay3
Contributor I

Hi @jeremyzhou,

We are using the Eval Board for testing.

We have written our custom code using UART. We tested it few times and it worked fine.

After that it started throwing the above mentioned error when we tried connecting in debug mode.

We tried running the same code with another EVAL kit and its working fine.

Regards,

Vinay. 

0 Kudos
Reply

2,707 Views
jeremyzhou
NXP Employee
NXP Employee

Hi
Thanks for your reply.
According to your description, I'd like to suggest you try the below two tricks to solve the debug errors.
1) Update the firmware of the on-board debugger of the MIMXRT1064;
2) Configure the SW7 to Serial Download mode, then connect the board to debug, after that, unplug the board and recover the SW7 to its previous position, connect the board to debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,693 Views
Vinay3
Contributor I

Hi @jeremyzhou ,

Could you please elaborate the procedure.

As I have tried keeping the board in SWD mode SW7 - 0001 

but it is still not connecting to flash the binary.

Regards,

Vinay

0 Kudos
Reply

2,655 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Sorry for the reply late.
The attachment consists of the OpenSDA bootloader and firmware application, you can give update the OpenSDA interface a try.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

2,647 Views
Vinay3
Contributor I

Hi @jeremyzhou ,

Could you please provide some detailed steps to Update the Bin files you have provided.

Regards,

Vinay

 

0 Kudos
Reply

2,643 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
To provide the fastest possible support, I'd highly recommend you refer to the application note.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply