IMXRT1064 Power Up sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT1064 Power Up sequence

跳至解决方案
3,147 次查看
alberto2
Contributor I

Hi,

the document "Hardware Development Guide for the MIMXRT1050/MIMXRT1060 Processor" clearly recommends respecting the power-up sequence showed in figure 1 of the document.

This would require the introduction of a DC/DC converter that is enabled through the PMIC_ON_REQ pin of the IMXRT1064 once the VDD_SNVS_IN is turned on (figure 2 of HW development guide).

However, on the IMXRT1064 datasheet, in section 4.2.1.1 Power-up sequence we can read: "VDD_SNVS_IN supply must be turned on before any other power supply or be connected (shorted) with VDD_HIGH_IN supply."

To my eyes, this is contradictory since if VDD_SNVS_IN is shorted to VDD_HIGH_IN, the power-up sequence showed in figure 1 of the hw development guide is not respected, since all the voltage references are being turned on at the same time.

Can you please clarify this?

Is it ok to short VDD_SNVS and VDD_HIGH_IN, or we need a sequencing element (DCDC or load switch enabled from pmic_on_req)?

Thank you.

Alberto

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
3,057 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Alberto, 

Can you please clarify this?

The statement "VDD_SNVS_IN supply must be turned on before any other power supply" applies only when you have a backup battery. If your application doesn't need a backup battery then you need to short VDD_SNVS_IN with VDD_HIGH_IN and in this case, the previous statement doesn't apply. 

Is it ok to short VDD_SNVS and VDD_HIGH_IN, or we need a sequencing element (DCDC or load switch enabled from pmic_on_req)?

It's ok if you short VDD_SNVS_IN and VDD_HIGH_IN, you don't need any extra circuitry. 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
3,058 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Alberto, 

Can you please clarify this?

The statement "VDD_SNVS_IN supply must be turned on before any other power supply" applies only when you have a backup battery. If your application doesn't need a backup battery then you need to short VDD_SNVS_IN with VDD_HIGH_IN and in this case, the previous statement doesn't apply. 

Is it ok to short VDD_SNVS and VDD_HIGH_IN, or we need a sequencing element (DCDC or load switch enabled from pmic_on_req)?

It's ok if you short VDD_SNVS_IN and VDD_HIGH_IN, you don't need any extra circuitry. 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复