IMXRT1064 FCB address offset in ref manual rev1 vs rev2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1064 FCB address offset in ref manual rev1 vs rev2

ソリューションへジャンプ
462件の閲覧回数
djarin
Contributor II

Hi,

The IMXRT1064 reference manual in Rev1 saying the FlexSPI Nor config parameters is located at offset 0x400. While in Rev2, there mentioned it is starting at offset 0x0.

Would like to know, since RM rev1 is published on year 2019, and if we have imxrt1064 mcu chip bought before year 2019, do we need to follow the offset address as 0x400?

also, we notice also imxrt1176 FCB offset address is 0x400, would like to understand why there is a change in imxrt1064, and why not make both consistent to same starting address?

Thank you

yeo_0-1715838811851.png

yeo_2-1715838883920.png

 

yeo_3-1715838972114.png

 

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
441件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @djarin 

  Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  Please refer to the newest RT1064RM:

https://www.nxp.com/webapp/Download?colCode=IMXRT1064RM

kerryzhou_0-1715853857121.png

RT1064 FCB is at the offset 0, don't compare with the RT1170, not the same series chip.

 

Wish it helps you!

Best Regards,

Kerry

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
442件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @djarin 

  Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

  Please refer to the newest RT1064RM:

https://www.nxp.com/webapp/Download?colCode=IMXRT1064RM

kerryzhou_0-1715853857121.png

RT1064 FCB is at the offset 0, don't compare with the RT1170, not the same series chip.

 

Wish it helps you!

Best Regards,

Kerry

 

0 件の賞賛
返信