IMXRT1010 Lpspi Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1010 Lpspi Flash

Jump to solution
211 Views
LuigiV
Contributor III

Hi,

I need to add a Nand Flash to my IMXRT1010 board lpspi to use it as a storage for my data; is there an example that explain how to write and read data to and from the flash ?

LuigiV_0-1716552665135.png

 

Thank you

 

Luigi

0 Kudos
Reply
1 Solution
180 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @LuigiV,

I'm afraid we only provide an example for the NOR flash component, which is in the SDK by the name of "flash_component_nor". This is not indented to be used with a NAND flash, of course, but could still be a good baseline to demonstrate the use of reading, writing and erasing to a flash device in general.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
1 Reply
181 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @LuigiV,

I'm afraid we only provide an example for the NOR flash component, which is in the SDK by the name of "flash_component_nor". This is not indented to be used with a NAND flash, of course, but could still be a good baseline to demonstrate the use of reading, writing and erasing to a flash device in general.

BR,
Edwin.

0 Kudos
Reply