IMXRT quad timers synchronization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT quad timers synchronization

Jump to solution
2,234 Views
dinartal
Contributor III

Is it possible to synchronize two quad timers to get 64bit timer with 8 capture inputs?

Labels (2)
0 Kudos
Reply
1 Solution
2,207 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Can we sync them together?
-- No, I'm afraid that they (two 64 bit quad timers) can't be synced.
I've answered your question in another post, please check it.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
2,223 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it possible to synchronize two quad timers to get 64bit timer with 8 capture inputs?
-- Actually, I'm not very clear with your question, so I was wondering if you can explain it again.
Looking forward to your reply.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,212 Views
dinartal
Contributor III

Let me try to explain my question: in IMXRT1020 we have two 64 bit quad timers TMR0 & TMR1 (4x16 cascaded). can we sync them together? it means that at any time there are same values in count registers. Count registers of both timers increase(decrese) simultinously.

0 Kudos
Reply
2,208 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Can we sync them together?
-- No, I'm afraid that they (two 64 bit quad timers) can't be synced.
I've answered your question in another post, please check it.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------