IMXRT UARTS Hardware RS485 and Smartcard operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT UARTS Hardware RS485 and Smartcard operation

1,122 Views
gredpath
Contributor III

I am trying to configure the RT10XX families to run RS485 with Hardware flow control and Smartcard operation.

Is this possible with these parts, an initial reading of the datasheet seems to suggest not. 

0 Kudos
Reply
2 Replies

946 Views
gredpath
Contributor III

Thanks Igor for the prompt reply, that answers the first part of the question, I checked this section of the document but I can't find support for ISO7816 smartcards using a UART, is there an app note to point me in the right direction for Smart card support?

Many thanks

George

0 Kudos
Reply

946 Views
igorpadykov
NXP Employee
NXP Employee

Hi George

for rs485 usage one can look at sect.39.2.2.4 Transceiver driver enable

using RTS_B i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply