Thanks for the reply,
I was looking into SBL and SFW projects.
i built the SBL project and tried to flash it on the board.
i. Use a micro USB cable to connect the EVKMIMXRT1170 board to the computer.
ii. Set the board to serial download mode.
iii. copied the sbl.bin file to the RT1050EVK drive detected by the windows
iv. Set the board to XIP mode
v. Reset the board.
but when I copy the sbl.bin file to the device, the explorer window closed automatically and when I rechecked the drive, I found the following error in the FILE.TXT file,
"The interface firmware FAILED to reset/halt the target MCU"
I would like to know how to flash the generated sbl.bin file?.