I2S Bidirectional communication via SAI2 in sln-local2-iot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2S Bidirectional communication via SAI2 in sln-local2-iot

6,433 Views
Blackpearl
Contributor II

Hi All,

I want to configure SAI2 in sln-local2-iot which is connected to DMIC in evk board as an interface for the communication with the host processor as follows.

Untitled Diagram-Page-3.drawio.png

Pinmuxing is done as follows. 

SAI2_TX_DATA   - GPIO_AD_B0_09-Jtag TDI pin
SAI2_TX_BCLK   - GPIO_AD_B0_05-Boot pin
SAI2_TX_SYNC - GPIO_AD_B0_04-Boot pin
SAI2_RX_DATA - GPIO_AD_B0_08 - DMIC pin

I Tried to record  DMIC data from SAI1  using SLN_AMP_Write() in the host processor via SAI2 .But data is not coming  out of the TX_DATA pin. Only BCLK and FYNC is coming. I am also using Jtag for debugging.Is that making any issue ?Could you please help  me to figure out the issue?What all configuration is needed for the SAI2 to communicate with the host processor?

 

 

0 Kudos
Reply
22 Replies

259 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Blackpearl ,

   As this case is no updated information for 1 month.

  If you have any questions, please create the new case, we can talk it in your new case.

  As we can't open the case more than one month, this case is opened for 2 month.

   Thanks a lot for your understanding.

Best Regards,

Kerry

0 Kudos
Reply

258 Views
Blackpearl
Contributor II

Hi @kerryzhou ,

Thanks for the response. I will open this as a new case.

0 Kudos
Reply