Hi,
i am using SDK_2_10_0_EVK-MIMXRT1060, IAR IDE 8.40.1
In the default SDK LPUART1 is configured for debug console but in my proto board i dont have LPUART1 so i have configured the LPUART7, i am not getting the console on terminal.
my processor is MIMXRT1062.
#define UART7_TX_IOMUXC IOMUXC_GPIO_SD_B1_08_LPUART7_TX
#define UART7_RX_IOMUXC IOMUXC_GPIO_SD_B1_09_LPUART7_RX
#define UART7_SW_IOMUXC IOMUXC_GPIO_SD_B1_06_GPIO3_IO06
#define UART7_SW_GPIO GPIO3
#define UART7_SW_GPIO_PIN 6U
//for Prototype Board using LPUART7
IOMUXC_SetPinMux(
UART7_232_TX_IOMUXC, /* GPIO_B0_08 is configured as LPUART7_TX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinMux(
UART7_232_RX_IOMUXC, /* GPIO_B0_09 is configured as LPUART7_RX */
0U); /* Software Input On Field: Input Path is determined by functionality */
IOMUXC_SetPinConfig(
UART7_232_TX_IOMUXC, /* GPIO_B0_08 PAD functional properties : */
0x10B0u);
IOMUXC_SetPinConfig(
UART7_232_RX_IOMUXC, /* GPIO_B0_09 PAD functional properties : */
0x10B0u);
IOMUXC_SetPinMux(
UART7_232_SW_IOMUXC,
0U);
IOMUXC_SetPinConfig(
UART7_232_SW_IOMUXC,
0xB0A9u);
please can you how to configure or any low level modification required please let me know.
Any input it would be grateful
Regards,
Naresh.
解決済! 解決策の投稿を見る。
Hi @naresh2 ,
Do you use the SDK hello_world project?
If yes, please also check the following area, do you modify it or not.
Then, it is the pinmux.c should configure the UART8 pins.
BTW, I highly suggest you use the new SDK SDK_2_11_1_EVK-MIMXRT1060 instead of the old one, you can download it from this link:
Best Regards,
kerry
Hi @naresh2 ,
Do you use the SDK hello_world project?
If yes, please also check the following area, do you modify it or not.
Then, it is the pinmux.c should configure the UART8 pins.
BTW, I highly suggest you use the new SDK SDK_2_11_1_EVK-MIMXRT1060 instead of the old one, you can download it from this link:
Best Regards,
kerry