I am looking to buy Ulink2 programmer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am looking to buy Ulink2 programmer?

1,141 Views
sanketkulkarni
Contributor III

I am looking to buy Ulink2 Programmer of ARM, the question comes to mind will it work on most of the boards? I want to a debugger which is universal and can work with any board. Ulink2 is in my bugdet, so I am asking this question. I am also looking for Segger Jlink as a universal debugger. Or there is another option in these regard?  

   Also, will Ulink2 will work i.mx 1020 board?

Tags (1)
0 Kudos
Reply
1 Reply

1,098 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sanket kulkarni

According to the Keil page, ULINK2 supports:

pastedImage_1.png

as long as the RT1020 is a Cortex M7, it does support this chip. you can find more information in their web page:

ULINK Debug Adapters 

Hope this information helps.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply