Hi,
On my RT1064-EVK I already made all steps from topic Hyper Flash on IMX RT1060-EVK does not work but have no result. Is it possible to boot from HyperFlash on this EVK?
p.s. HyperFlash IC after hardware resistor modification (R356, R361-R366) works fine with the example from SDK_2.6.1_EVK-MIMXRT1064\boards\evkmimxrt1064\driver_examples\flexspi\hyper_flash\polling_transfer.
I also configured all the changes of registers but example code(sdk) is not working for me. Can you please guide me?
Hello,
>>Is it possible to boot from HyperFlash on this EVK?
Yes, It is possible.For the detail please refer to the application note https://www.nxp.com/docs/en/application-note/AN12107.pdf.
Hi, fangfang.
Thank you for recomendation. I saw this AppNote.
Unfortunately, this is so in theory. . Did you manage to get the result that interests me in practice on this RT1064-EVK? I emphasize, not on the RT1050-EVK and not on the RT1060-EVK.