How to use the QSPI flash in Gui-Guider with imxrt1050?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use the QSPI flash in Gui-Guider with imxrt1050?

跳至解决方案
1,026 次查看
mperez1
Contributor II

Hello there,

I just discover the Gui-Guider application to use with lvgl. I'm able to generate a project and add widgets. But my problem is when i'm trying to load the application in the board. I have a custom board with a QSPI flash instead of a Hyperflash. There is any way to change this in the Gui-Guider? Even changing any file in the Gui-Guider root?

Thank you in advance,

Miguel

0 项奖励
回复
1 解答
1,009 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Miguel,

Booting from QSPI depends on the project configuration. The MCUXpresso SDK example is intended to boot from Hyperflash, please check the following application note for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

Best regards,

Felipe

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,010 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Miguel,

Booting from QSPI depends on the project configuration. The MCUXpresso SDK example is intended to boot from Hyperflash, please check the following application note for more details.

https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf

Best regards,

Felipe

0 项奖励
回复