How to use blhost to generate image with plain CRC on bootup enabled?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use blhost to generate image with plain CRC on bootup enabled?

1,128 Views
pcpro1789
Contributor III

The title says it all.  How can blhost be used to generate an image with the plain CRC check enabled?  We're using load to RAM, not run in place.

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,083 Views
pcpro1789
Contributor III

@Gavin_Jia Do I understand correctly that to use blhost to get the image CRC, the only way requires programming the target device and reading back the information from the target device?

0 Kudos
Reply

1,074 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @pcpro1789 

The CRC is added through the nxpimage(a python tool). It is unnecessary to program the image to the MCU after completion.

0 Kudos
Reply

1,109 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @pcpro1789 ,

Thanks for your questions!

1. First, we need to generate an image that runs in RAM, not XIP. And convert it to S-Record type.

Gavin_Jia_0-1733825262347.png

Gavin_Jia_1-1733825328354.png

 

2. Then, we need to generate the corresponding image according to your needs. this step requires the nxpimage tool, which you are advised to modify in the graphical interface in SPT. Its corresponding command line underlying command will be shown in the log, you can record and parse it.

Gavin_Jia_2-1733825489510.png

 

3. Finally, it's time to use blhost. build the FCB, configure the memory, flash the image. and so on. Again, the underlying commands are logged in the log. After I parsed it, it is divided into the following steps:

  • blhost -t 2000 -p COM75,115200 -j -- get-property 1 0    Check connection
  • blhost -t 50281 -p COM75,115200 -j -- flash-erase-region 0x08000000 28168 9   Erase flash
  • blhost -t 5000 -p COM75,115200 -j -- fill-memory 0x0010C000 4 0xF000000F word   Setup FCB
  • blhost -t 5000 -p COM75,115200 -j -- configure-memory 9 0x0010C000   Configure memory
  • blhost -t 5000 -p COM75,115200 -j -- write-memory 0x08000600 "image_version.bin" 0  Write version
  • blhost -t 5000 -p COM75,115200 -j -- write-memory 0x08001000 "evkmimxrt685_gpio_led_output.bin" 0    Write application
 
Each command uses the blhost tool to communicate with the device and perform the required operations to write the image.

 

 

 

0 Kudos
Reply