How to support UAC2.0 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to support UAC2.0 ?

3,913件の閲覧回数
nickcai
Contributor II

Hello,

   On I.MX RT1050 EVK with FreeRTOS.Want to support USB AUDIO CLASS 2.0,what need to do ? who can offer DEMO ?

tks.

ラベル(1)
タグ(1)
2 返答(返信)

3,112件の閲覧回数
EdSutter
Senior Contributor II

Hi, I am about to embark on a multi-channel audio/usb project that requires UAC2.0 also... As I dig into the SDK for answers, @nick, did you find support for UAC2.0 (which implies HighSpeed USB) in the SDK?

Thanks in advance,

Ed

0 件の賞賛
返信

3,112件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi nick

please check usb audio examples included in

MCUXpresso SDK

i.MX RT1050 Evaluation Kit|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信