Hi,
There are found APIs in fsl_dsp.h. They are
I have tried DSP_Stop() and DSP_Start(). The results seem pause and resume the HIFI DSP core. I haven't found the reset.
If switch to DSP_Deinit() and DSP_Init(), have to re-copy the DSP image to the memory regions which are assigned to DSP code.
Is there any method to reset HIFI DSP core of RT685 without re-copying the DSP image?
已解决! 转到解答。
Hi @JerryQian_132 ,
You can refer to section 4.5.3.2 in user manual. There is a reset contol0 register which can reset DSP.
Regards,
jing