How to port NFC PN5180 with i.MX RT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to port NFC PN5180 with i.MX RT1050

1,536 Views
yen_chen
Contributor III

Hi,all

I need to port PN5180 to RT1050.

Could anyone  support porting guide ?

I add DAL,NxpNfcRdLib,intfs,phOsal for RT1050 now.

If I use PN5180, which file I need to modify ?

 

0 Kudos
Reply
3 Replies

1,528 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, we do not have specific porting guide for PN5180 but I think you can use this guide as reference.

NFC Reader Library Porting to i.MX RT1050 - NXP Community

Best regards,

Felipe

0 Kudos
Reply

1,512 Views
yen_chen
Contributor III

Hi @FelipeGarcia 

If I want to set PHDRVIER_PIN in the DAL/boards

How to know the vaule and set ?

 

Br,

Yen

 

0 Kudos
Reply

1,499 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Yen,

You can see the pins needed by PNEV5180B in the following document. On the RT side you will need to set the pins you are going to use, there are no specific pins just verify that they accomplish the desired functionality.

https://www.nxp.com/docs/en/application-note/AN11908.pdf

Best regards,

Felipe

0 Kudos
Reply