Hi,
We want to use two image primary and secondary.
We want to shift primary to secondary and vice versa (8.6.4.5 Redundant boot support for expansion device - Reference manual) how can we access PERSIST_SECONDARY_BOOT in our program ?
This case we need to use external qspi (or) internal flash is sufficient ?
Any other suggestion is there from nxp side ?
Thanks & Regards
Vasu
Hi vasu dhevan
The Persist_Secondary_Boot bit is located in the SRC_GPR10[30] field. If you require to implement OTA, you can use the secondary bootloader that we provide with the SDK as a reference for your implementation of the OTA.
You will require an external module for the wireless part, depending on if you going to use BLE, Wifi, NFC, etc, I recommend you to create a new question in the community space for that technology.
Best regards
Jorge Alcala
Dear Jorge,
Thank you for your response.
OTA why we need go with wireless part already ethernet available ?
Internal flash contains primary program QSPI 8MB contains secondary program this possible remaining qspi space our application data like configuration and certificates.
Can we possible shift boot primary image from internal flash and secondary image form external qspi at any time ?
If we kept two images in external qspi can we use internal flash our application data storage(config data) purpose ?
Thanks & Regards
Vasu
Hi Vasudhevan G
Could you clarify your questions:
Can we possible shift boot primary image from internal flash and secondary image form external qspi at any time ?
The Persist_Secondary_Boot bit only work in a boot interface. The internal flash memory and the external memory uses two interface, so you cannot use the Persist_Secondary_Boot bit with internal  boot and external boot.
If we kept two images in external qspi can we use internal flash our application data storage(config data) purpose ?
Yes, you can use it as data storage, but those values are not designed to change constantly as it is a flash memory.
Best regards
Jorge Alcala
Hi Jorge,
Sorry for the late reply.
NXP side any plan is there imxrt1064 ota example project in upcoming sdk release ?
Thanks & Regards
Vasu