How to flash(internal) 1064 using mfg tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash(internal) 1064 using mfg tool

ソリューションへジャンプ
2,898件の閲覧回数
vasudhevan
Contributor V

Hi,

      If we use JTAG how to implement secure boot using internal flash ?

      How to flash dual image 1064 internal flash ?

      How can we use mfg tool flashing internal flash ?

 

Thanks & Regards 

       Vasu

0 件の賞賛
返信
1 解決策
2,754件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vasudhevan G,

   You need to enter the serial download mode at first, then use the following UART pins to connect your RT chip and donwload it.pastedImage_1.png

About the download,  I suggest you use our MCUBootUtility tool to download it, it's very easy to use:

https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v2.1.0

the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

You can try it at first.

If you still have questions about it, please kindly let me know.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,754件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vasudhevan G ,

   Answer your questions:

1. If we use JTAG how to implement secure boot using internal flash ?

Answer:

  You can refer to this application note at first:

Secure JTAG for i.MXRT10xx

2.      How to flash dual image 1064 internal flash ?

Answer: I don't fully understand your questions, as I know, RT1064 just have one internal flash. What do you mean the dual image? Just put in the different range? If yes, then I think you can merge two image together in one image file, then download it.

3.      How can we use mfg tool flashing internal flash ?

Answer: You can refer to this application note:

How to Enable Boot from QSPI Flash

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,754件の閲覧回数
vasudhevan
Contributor V

Hi Kerry,

    We are new to imxrt crossover family.

    2) Dual image means dual binary file flashing at same time one is primary and another one is factory restore.

    3) How to enable boot from QSPI Flash - this document related to external spi flash but i am asking flashing internal flash using mfg tool ?

Thanks & Regards

       Vasu

0 件の賞賛
返信
2,754件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vasudhevan G,

  Good question!

  About the boot from QSPI flash, if you check more details about RT1064 internal flash, you will find the RT1064 internal flash is just one winbond W25Q32JV chip put in the RT1064 chip, so the external flexSPI flash operation is totally the same as your internal flash.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,754件の閲覧回数
vasudhevan
Contributor V

Hi Kerry,

   Thank you for your reply,

 How to flash imxrt 1064 internal flash using UART1 ?

   Thanks & Regards

           Vasu

0 件の賞賛
返信
2,755件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vasudhevan G,

   You need to enter the serial download mode at first, then use the following UART pins to connect your RT chip and donwload it.pastedImage_1.png

About the download,  I suggest you use our MCUBootUtility tool to download it, it's very easy to use:

https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v2.1.0

the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

You can try it at first.

If you still have questions about it, please kindly let me know.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,754件の閲覧回数
vasudhevan
Contributor V

Hi Kerry,

  Thank you for your response.

   Further doubt and issue let you know.

Thanks & Regards 

       Vasu

0 件の賞賛
返信