How to enter SEMC SDRAM into low power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enter SEMC SDRAM into low power

409件の閲覧回数
rjengr
Contributor I

We are using a imxrt106F, with VDD_HIGH_IN, SNVS_IN, and DCDC_IN tied together. However the issue we see is entering into SNVS does not automatically put the SDRAM into low power mode as our SDRAM is constantly powered. We are seeing very high power consumption. How can we put the SDRAM into low power mode?

0 件の賞賛
返信
1 返信

370件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

If the SDRAM has a low power mode then you need to enter the command to send it to low power before setting the mcu at SNVS mode.

Ideally, SDRAM is powered-off on SNVS mode since external DC/DC(which powers SDRAM) is turned off.

Omar_Anguiano_0-1727894242690.png

Best regards,
Omar

0 件の賞賛
返信