Hi NXP,
I was trying to stream a custom camera which has an ISP using RT1170 as a part of that I was able to do the following:
1. Able to read and write to the camera using I2c.
2. The camera is initializing and sending the test pattern frames (Confirmed it by reading the frame count register in the ISP).
The problem is:
From camera side I was able to debug the faults related to it. By reading its fault registers.
But I was unable to debug on the CSI2 receiver side in the board.
I have followed the AN13573 and Tried to debug it. But when I tried to read the MIPI status register its always giving "0" as shown below.
MIPI_Err PPI_ERRSOT_HS =0,
MIPI_Err PPI_ERRSOTSYNC_HS =0,
MIPI_Err PPI_ERRESC =0,
MIPI_Err PPI_ERRSYNCESC =0,
MIPI_Err PPI_ERRCONTROL =0,
MIPI_Err IRQ_STATUS =0,
MIPI_Err BIT_ERR =0,
I was unable to proceed further with this. Do we have any anyway to check whether we are getting frame buffers on MIPI CSI receiver side. Could anyone be able to help me regarding this problem?
Thanks & Regards,
Ragnar.