How to connect MCU Boot Utility to iMXRT105 via UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect MCU Boot Utility to iMXRT105 via UART

2,179 Views
namht
Contributor III

Hi all,

I'm working on custom board using MIMXRT1052CVL5B. I was config "SEC_CFG[1] = 1"  in "MCU Boot Utility v3.4.0" software via UART:

thanhnambka_0-1650938182359.png

After i Save->Burn->Reboot my board, i cannot connect to "MCU Boot Utility" via UART. When i connect, this messeger show:

thanhnambka_2-1650938615496.png

 

My question: "How to connect MCU Boot Utility to iMXRT105 via UART".

 

 

 

Labels (1)
3 Replies

2,149 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
1) Can you help me to find "Serial (8 digits)" and "key_pass (text)" ?
-- Please check it under the NXP-MCUBootUtility-master\gen\hab_cert directory.
Plus, please select the HAB Signed Image Boot prior to clicking the Connect to ROM and you can give it a try.

jeremyzhou_0-1651041576267.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,169 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, the HAB secure boot has already been enabled after burning the SEC_CFG[1], secondly, it needs to import keys for the MCUbootUtility tool, and last, it should select the HAB Signed Image Boot.

jeremyzhou_0-1650944528146.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply

2,160 Views
namht
Contributor III

Hi, thanks you for your reply.

I readed MCU Boot Utility's manual, and finded instruction Enable HAB signature authentication:

 

thanhnambka_1-1650956654889.png

 

However, i never set a keys for imxrt, therefore i don't know keys. Can you help me to find "Serial (8 digits)" and "key_pass (text)" ?

0 Kudos
Reply