How to build yocto image for iMX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to build yocto image for iMX53

2,675 Views
kman_devnull
Contributor I

I am new to imx based processors.

I have an imx53 eval board, I need to build an yocto image which supports:

+ lvds 7 inch display

+ qt5

+ qt webkit

How do I get started ?

Tags (1)
0 Kudos
Reply
2 Replies

2,201 Views
igorpadykov
NXP Employee
NXP Employee

Hi kman

one can review below links describing i.MX53 support:

Submit i.MX53 & i.MX28 Linux kernel patches 

https://community.nxp.com/thread/462874 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,201 Views
kman_devnull
Contributor I

Hi,

Thanks.

Being a newbie - though those links are very informative - tt doesn't tell

me how to get a yocto image/build going for:

i.MX53 with:

1) lvds(7 inch display)

2) qt5 & qtwebkit

3) Also what versions of Yocto / or the different layers that are required.

Please help.

0 Kudos
Reply