How to add program protection function to RT1060 and RT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add program protection function to RT1060 and RT1064

2,676 Views
lw3
Contributor I

How to add program protection function to RT1060 and RT1064

Prohibit reading programs through SWD or serial or USB methods

Can encryption function be enabled

Can the flash run normally when switched to another MCU

How to Prevent Copying Flash and Replacing with Other RT1060 MCUs from Running Properly

0 Kudos
Reply
8 Replies

2,651 Views
lw3
Contributor I

After adding read protection to the jlink swd interface

Can we use the swd port of jlink to download new programs again in the future

0 Kudos
Reply

2,644 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

Yes, please refer to AN12419.

 

Regards,

0 Kudos
Reply

2,617 Views
lw3
Contributor I
Can you give me the download connection for AN12419
0 Kudos
Reply

2,608 Views
jingpan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,557 Views
lw3
Contributor I
I'll study how to use it
0 Kudos
Reply

2,557 Views
lw3
Contributor I
Thank you
0 Kudos
Reply

2,661 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

To prevent unauthorized read from SWD/JTAG, you should enable SJTAG.

To prevent copy code, you should use BEE and encrypt the code in flash.

 

Regards,

Jing

0 Kudos
Reply