Hard Fault error on MIMXRT1064CVL5B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard Fault error on MIMXRT1064CVL5B

800 Views
kksakthi
Contributor I

 

We using the MIMXRT1064CVL5B in our design, we facing the some problem in software development. please conform  why   Hard Fault error come, its based on Hardware design? how to solve it, please help me.

0 Kudos
Reply
3 Replies

762 Views
kksakthi
Contributor I

We need your help regarding the above, please help us as soon as possible.

Regards,

Sakthi,

Embedded Hardware Engineer,

RGBSI,

Bangalore.

0 Kudos
Reply

763 Views
kksakthi
Contributor I

Hi thanks for your replied, we used customized our source code but hard fault problem solved. we facing some  other problem now.

Microcontroller: iMXRT1064

 

In our custom board, we are using most of the boot configuration pins for other functionalities like I2C, SPI, and GPIO inputs with pullups.

 

During the boot, the state of these pins affects the normal boot.

 

From the reference manual, we came to know that, we can set the BT_FUSE_SEL eFuse to override the boot configuration pins.

 

Our custom board doesn't have a USB interface to configure the eFuses.

 

We found an alternative from the NXP's forum, to burn the fuses using OCOTP. We used the following code. When we read the fuse address 0x460, we are getting the value 0x00000010. But still the state of boot config GPIOs affects the boot.

 

#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_ocotp.h"
#include "fsl_debug_console.h"

 

#define EXAMPLE_OCOTP_SHADOW_REGISTER_READ_ENABLE         1U
#define EXAMPLE_OCOTP_SHADOW_REGISTER_WRITE_ENABLE         0U

 

#if EXAMPLE_OCOTP_SHADOW_REGISTER_READ_ENABLE || EXAMPLE_OCOTP_SHADOW_REGISTER_WRITE_ENABLE

 

#ifndef EXAMPLE_OCOTP_FUSE_MAP_ADDRESS
#define EXAMPLE_OCOTP_FUSE_MAP_ADDRESS                     0x460
#endif

 

#ifndef EXAMPLE_OCOTP_FUSE_WRITE_VALUE
#define EXAMPLE_OCOTP_FUSE_WRITE_VALUE                     0x00000010
#endif

 

#endif

 

int main(void)
{
    uint32_t version;

 

    /* Init hardware*/
    BOARD_ConfigMPU();
    BOARD_InitBootPins();
    BOARD_InitBootClocks();
    BOARD_InitDebugConsole();

 

    PRINTF("OCOTP Peripheral Driver Example\r\n\r\n");

 

#if (defined(FSL_FEATURE_OCOTP_HAS_TIMING_CTRL) && FSL_FEATURE_OCOTP_HAS_TIMING_CTRL)
    OCOTP_Init(OCOTP, EXAMPLE_OCOTP_FREQ_HZ);
#else
    OCOTP_Init(OCOTP, 0U);
#endif

 

    /* Get the OCOTP controller version. */
    version = OCOTP_GetVersion(OCOTP);
    PRINTF("OCOTP controller version: 0x%08X\r\n\r\n", version);

 

#if EXAMPLE_OCOTP_SHADOW_REGISTER_READ_ENABLE || EXAMPLE_OCOTP_SHADOW_REGISTER_WRITE_ENABLE
    status_t status   = kStatus_Success;
    uint32_t fuseData = 0U;

 

    status = OCOTP_ReadFuseShadowRegisterExt(OCOTP, EXAMPLE_OCOTP_FUSE_MAP_ADDRESS, &fuseData, 1);

 

    if (status != kStatus_Success)
    {
        PRINTF("Could not read fuse data\r\n");
        while (1)
            ;
    }

 

    PRINTF("The origin value of fuse address 0x%02X is 0x%08X\r\n", EXAMPLE_OCOTP_FUSE_MAP_ADDRESS, fuseData);
#endif

 

#if EXAMPLE_OCOTP_SHADOW_REGISTER_WRITE_ENABLE
    status = OCOTP_WriteFuseShadowRegister(OCOTP, EXAMPLE_OCOTP_FUSE_MAP_ADDRESS, EXAMPLE_OCOTP_FUSE_WRITE_VALUE);

 

    if (kStatus_Success == status)
    {
        PRINTF("OCOTP Write operation success!\r\n");

 

        status = OCOTP_ReadFuseShadowRegisterExt(OCOTP, EXAMPLE_OCOTP_FUSE_MAP_ADDRESS, &fuseData, 1);

 

        if (status != kStatus_Success)
        {
            PRINTF("Could not read fuse data\r\n");
            while (1)
                ;
        }

 

        PRINTF("The new value is 0x%08X\r\n", fuseData);
    }
    else
    {
        PRINTF("OCOTP write operation failed. Access deny!\r\n");
    }
#endif

 

    while (1)
    {
    }
}

0 Kudos
Reply

792 Views
jay_heng
NXP Employee
NXP Employee

Which code will cause hardfault? your application only or any example from SDK?

0 Kudos
Reply