FlexSPI initialization fails when running from XIP flash on iMXRT1040

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexSPI initialization fails when running from XIP flash on iMXRT1040

608件の閲覧回数
rd24
Contributor III

Board - iMXRT1040-EVK, SDK - mcuXpresso SDK v25.03.00

Hi,

I am working on my custom application which uses FlexSPI. I followed the "flexspi/nor/edma" example to develop my code. The example is working fine on the EVK, both from XIP and RAM.

My application is working fine only when I run it from RAM, but from XIP the behaviour is erratic. In the init function sometimes it hangs in this while loop.

/* Waiting for bus idle only when FLEXSPI enabled. */
if ((base->MCR0 & FLEXSPI_MCR0_MDIS_MASK) != FLEXSPI_MCR0_MDIS_MASK)
{
    /* Make sure flexspi bus idle before change its clock setting. */
    while (!FLEXSPI_GetBusIdleStatus(base))
    {
    }
}

 

When I step debug through the while loop, it hangs or crashes at:

FLEXSPI_Init(base, &config);

 

My application is using FreeRTOS. I have tried calling the init function from main() before starting the scheduler, as well as from a thread. It uses other peripherals like CAN, SPI but I have disabled them, still I see the same behaviour.

Below is my clock configuration called from main()

static void clockInit(void)
{
    /* Enable the external 24 MHz oscillator. */
    CLOCK_SetXtalFreq(24000000U);
    CLOCK_InitExternalClk(0);
    CLOCK_SwitchOsc(kCLOCK_XtalOsc);

    /* The PLL3 480 MHz clock (aka USB1 PLL) is derived from the
       external oscillator with a fixed multiplier of 20. */
    CLOCK_SetMux(kCLOCK_Pll3SwMux, 0); /* 0 = Derive from main clock */

    /* The UART clock is derived from PLL3, with a static divider of 6
       plus a variable divider of 1. */
    CLOCK_DisableClock(kCLOCK_Lpuart1);
    CLOCK_SetDiv(kCLOCK_UartDiv, 0); /* 0 = Divide by 1 */
    CLOCK_SetMux(kCLOCK_UartMux, 0); /* 0 = Derive from PLL3 */

    /* Disable Flexspi2 clock gate. */
    CLOCK_DisableClock(kCLOCK_FlexSpi2);
    /* Set FLEXSPI2_PODF. */
    CLOCK_SetDiv(kCLOCK_Flexspi2Div, 1);
    /* Set Flexspi2 clock source. */
    CLOCK_SetMux(kCLOCK_Flexspi2Mux, 1);

    /* Init ARM PLL. */
    CLOCK_InitArmPll(&armPllConfig_BOARD_BootClockRUN);
    
    /* Init System PLL. */
    CLOCK_InitSysPll(&sysPllConfig_BOARD_BootClockRUN);
    /* Init System pfd0. */
    CLOCK_InitSysPfd(kCLOCK_Pfd0, 27);
    /* Init System pfd1. */
    CLOCK_InitSysPfd(kCLOCK_Pfd1, 16);
    /* Init System pfd2. */
    CLOCK_InitSysPfd(kCLOCK_Pfd2, 24);
    /* Init System pfd3. */
    CLOCK_InitSysPfd(kCLOCK_Pfd3, 16);
}

 

What is the issue here? I need some ideas on what I should be trying to find the issue.

Thanks

 

タグ(3)
0 件の賞賛
返信
4 返答(返信)

489件の閲覧回数
rd24
Contributor III

I debugged further and found that the erase and write commands are crashing (HardFault) in continuous run mode only. If I step debug through these functions then they work. The read command is working fine for me, I am able to read and print the values.

Any suggestions what might be the issue with erase and write? I am still confused how these are working in step debug mode.

Regards

0 件の賞賛
返信

407件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi ,

Completely referencing the project in the SDK should be unlikely to result in the situation you describe, check a few key points:

DCACHE/ICACHE handling should be consistent with that in the SDK;

ENABLE_RAM_VECTOR_TABLE macro is properly configured;

 

Best regards,
Gavin

 

0 件の賞賛
返信

588件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @rd24 ,

Thanks for your interest in NXP MIMXRT series!

You can find this folder in the project file of the SDK example:

Gavin_Jia_0-1749094351829.png

It controls the linkfile generated by the IDE, resulting in the following final generated image:

Gavin_Jia_1-1749094423704.png

 

That is, even though the project is XIP, the FlexSPI related code is still executed in RAM.

Best regards,
Gavin

 

0 件の賞賛
返信

520件の閲覧回数
rd24
Contributor III

Hi @Gavin_Jia ,

I am using the armgcc SDK on Linux, so I modified my linker script as per "MIMXRT1042xxxxx_flexspi_nor.ld". Now if I step debug through the application it works fine. I am able to initialize, then read, program and erase. But if I run the program crashes, i.e. HardFault_Handler gets called at "FLEXSPI_SoftwareReset()" inside the init function.

Any idea what could cause the program to crash?

0 件の賞賛
返信