FlexSPI configuration block (flexspi_nor_config_t) v1.4.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexSPI configuration block (flexspi_nor_config_t) v1.4.0

Jump to solution
2,143 Views
gavin5342
Contributor III

My board boots from QSPI NOR flash through FlexSPI.  I would like to change the FlexSPI LUT configuration that is configured by ROM to be able to use the extended status registers in my flash device so I am changing the content of the flexspi_nor_config_t qspiflash_config struct that gets linked to .boot_hdr.

The IMXRT1050RM document tells me about version 1.1 - 0x56010100 of the FlexSPI Configuration Block in table 9-14, but the SDK is using 0x56010400.

The LUT sequences end up in different LUT locations to the one that I would expect from table 9-15.  Is this because the version is different?  Where can I find the mapping of sequences in qspiflash_config.memConfig.lookupTable to the LUT in FLEXSPI?  What changes from v1.1 to v1.4 of the configuration block?

0 Kudos
Reply
1 Solution
2,066 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @gavin5342 ,

   To the SDK FCB, it will all copied to the FlexSPI LUT with the ROM.

   You can use the SDK example:

const flexspi_nor_config_t
    hyperflash_config =
        {
            .memConfig =
                {
                    .tag                = FLEXSPI_CFG_BLK_TAG,
                    .version            = FLEXSPI_CFG_BLK_VERSION,
                    .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
                    .csHoldTime         = 3u,
                    .csSetupTime        = 3u,
                    .columnAddressWidth = 3u,
                    // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
                    .controllerMiscOption =
                        (1u << kFlexSpiMiscOffset_DdrModeEnable) | (1u << kFlexSpiMiscOffset_WordAddressableEnable) |
                        (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DiffClkEnable),
                    .deviceType         = kFlexSpiDeviceType_SerialNOR,
                    .sflashPadType      = kSerialFlash_8Pads,
                    .serialClkFreq      = kFlexSpiSerialClk_133MHz,
                    .lutCustomSeqEnable = 0x1,
                    .sflashA1Size       = 64u * 1024u * 1024u,
                    .dataValidTime      = {15u, 0u},
                    .busyOffset         = 15u,
                    .busyBitPolarity    = 1u,
                    .lookupTable =
                        {
                            // Read LUTs
                            [0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_DDR, FLEXSPI_8PAD, 0x0C),
                            [2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),

                            // Read Status LUTs
                            // 0
                            [4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 1 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 1 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 1 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x70),

                            // 1
                            [4 * 2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 2 + 1] =
                                FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_RWDS_DDR, FLEXSPI_8PAD, 0x0B),
                            [4 * 2 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x4, STOP, FLEXSPI_1PAD, 0x0),

                            // Write Enable LUTs
                            // 0
                            [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 3 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 3 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 3 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 1
                            [4 * 4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 4 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 4 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 4 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // Erase Sector LUTs
                            // 0
                            [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 5 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 5 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 5 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),

                            // 1
                            [4 * 6 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 6 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 6 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 6 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 2
                            [4 * 7 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 7 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 7 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 7 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // 3
                            [4 * 8 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 8 + 1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 8 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x30, STOP, FLEXSPI_1PAD, 0x0),

                            // Page Program LUTs
                            // 0
                            [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 9 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 9 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 9 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xA0),

                            // 1
                            [4 * 10 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 10 + 1] =
                                FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, WRITE_DDR, FLEXSPI_8PAD, 0x80),

                            // Erase Chip LUTs
                            // 0
                            [4 * 11 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 11 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 11 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 11 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),

                            // 1
                            [4 * 12 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 12 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 12 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 12 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 2
                            [4 * 13 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 13 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 13 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 13 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // 3
                            [4 * 14 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 14 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 14 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 14 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x10),
                        },
                    // LUT customized sequence
                    .lutCustomSeq = {{
                                         .seqNum   = 0,
                                         .seqId    = 0,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 1,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 3,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 4,
                                         .seqId    = 5,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 9,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 4,
                                         .seqId    = 11,
                                         .reserved = 0,
                                     }},
                },
            .pageSize           = 512u,
            .sectorSize         = 256u * 1024u,
            .ipcmdSerialClkFreq = 1u,
            .serialNorType      = 1u,
            .blockSize          = 256u * 1024u,
            .isUniformBlockSize = true,
};

 

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
3 Replies
2,103 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @gavin5342 ,

   Thanks for your interest in the NXP MIMXRT product, I would like to provide service for you.

    For the FCB, I highly recommend you refer to the newest RT1050 SDK code, that is the newest one.

    To the RM, the doc is a little old, so I still recommend you refer to SDK code.

 

Wish it helps you!

Best Regards,

kerry

0 Kudos
Reply
2,095 Views
gavin5342
Contributor III

Thanks Kerry.  I can see the structure in the SDK, but can you tell me how entries in the FCB lookupTable get copied to the FLEXSPI LUT?  I know for sure that not all entries get copied across, but I would like to know so that I can fill the LUT out at boot without having to update it again after boot (especially risky as I used XIP).  Where can I find the updated information?

Gavin

0 Kudos
Reply
2,067 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @gavin5342 ,

   To the SDK FCB, it will all copied to the FlexSPI LUT with the ROM.

   You can use the SDK example:

const flexspi_nor_config_t
    hyperflash_config =
        {
            .memConfig =
                {
                    .tag                = FLEXSPI_CFG_BLK_TAG,
                    .version            = FLEXSPI_CFG_BLK_VERSION,
                    .readSampleClksrc=kFlexSPIReadSampleClk_ExternalInputFromDqsPad,
                    .csHoldTime         = 3u,
                    .csSetupTime        = 3u,
                    .columnAddressWidth = 3u,
                    // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
                    .controllerMiscOption =
                        (1u << kFlexSpiMiscOffset_DdrModeEnable) | (1u << kFlexSpiMiscOffset_WordAddressableEnable) |
                        (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DiffClkEnable),
                    .deviceType         = kFlexSpiDeviceType_SerialNOR,
                    .sflashPadType      = kSerialFlash_8Pads,
                    .serialClkFreq      = kFlexSpiSerialClk_133MHz,
                    .lutCustomSeqEnable = 0x1,
                    .sflashA1Size       = 64u * 1024u * 1024u,
                    .dataValidTime      = {15u, 0u},
                    .busyOffset         = 15u,
                    .busyBitPolarity    = 1u,
                    .lookupTable =
                        {
                            // Read LUTs
                            [0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_DDR, FLEXSPI_8PAD, 0x0C),
                            [2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP, FLEXSPI_1PAD, 0x0),

                            // Read Status LUTs
                            // 0
                            [4 * 1 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 1 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 1 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 1 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x70),

                            // 1
                            [4 * 2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xA0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 2 + 1] =
                                FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, DUMMY_RWDS_DDR, FLEXSPI_8PAD, 0x0B),
                            [4 * 2 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x4, STOP, FLEXSPI_1PAD, 0x0),

                            // Write Enable LUTs
                            // 0
                            [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 3 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 3 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 3 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 1
                            [4 * 4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 4 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 4 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 4 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // Erase Sector LUTs
                            // 0
                            [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 5 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 5 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 5 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),

                            // 1
                            [4 * 6 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 6 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 6 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 6 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 2
                            [4 * 7 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 7 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 7 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 7 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // 3
                            [4 * 8 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 8 + 1] = FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 8 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x30, STOP, FLEXSPI_1PAD, 0x0),

                            // Page Program LUTs
                            // 0
                            [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 9 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 9 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 9 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xA0),

                            // 1
                            [4 * 10 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, RADDR_DDR, FLEXSPI_8PAD, 0x18),
                            [4 * 10 + 1] =
                                FLEXSPI_LUT_SEQ(CADDR_DDR, FLEXSPI_8PAD, 0x10, WRITE_DDR, FLEXSPI_8PAD, 0x80),

                            // Erase Chip LUTs
                            // 0
                            [4 * 11 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 11 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 11 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 11 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x80),

                            // 1
                            [4 * 12 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 12 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 12 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 12 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),

                            // 2
                            [4 * 13 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 13 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),
                            [4 * 13 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x02),
                            [4 * 13 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x55),

                            // 3
                            [4 * 14 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x0),
                            [4 * 14 + 1] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0xAA),
                            [4 * 14 + 2] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x05),
                            [4 * 14 + 3] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x0, CMD_DDR, FLEXSPI_8PAD, 0x10),
                        },
                    // LUT customized sequence
                    .lutCustomSeq = {{
                                         .seqNum   = 0,
                                         .seqId    = 0,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 1,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 3,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 4,
                                         .seqId    = 5,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 2,
                                         .seqId    = 9,
                                         .reserved = 0,
                                     },
                                     {
                                         .seqNum   = 4,
                                         .seqId    = 11,
                                         .reserved = 0,
                                     }},
                },
            .pageSize           = 512u,
            .sectorSize         = 256u * 1024u,
            .ipcmdSerialClkFreq = 1u,
            .serialNorType      = 1u,
            .blockSize          = 256u * 1024u,
            .isUniformBlockSize = true,
};

 

Best Regards,

Kerry

0 Kudos
Reply