FlexIO3 different than FlexIO 1 & 2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexIO3 different than FlexIO 1 & 2?

1,205 次查看
markflamer
Contributor I

Hi, I posted this question last week but just realized I posted it to the wrong forum. So, Im posting it again here. I am currently using the FlexIO2 module along with eDMA on a few projects. So far it has all worked out very well. Yesterday I noticed this diagram in the document "IMXRT1060RM Rev. 3, 07/2021". It's interesting that FlexIO3 is shown here as tightly coupled with the CPU, while FlexIO modules 1 & 2 are located with the rest of the peripherals. I have not noticed any mention of this difference in chapter 50 on FlexIO.

How is the FlexIO3 module different than FlexIO 1 & 2?

Thanks!

markflamer_0-1654006993915.png

 

0 项奖励
回复
1 回复

1,197 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @markflamer ,

Please see Figure 28-1 in RM. The ARM core can access FlexIO3 faster than FlexIO1/2. To access FlexIO1/2, the route is AXI->AIPS->FlexIO1/2. But to access FlexIO3, it is more directly. And AXI speed is 132M maximum, but the AHBP is low-latency and much faster.

 

Regards,

Jinf

0 项奖励
回复