FlexIO3 different than FlexIO 1 & 2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexIO3 different than FlexIO 1 & 2?

1,210件の閲覧回数
markflamer
Contributor I

Hi, I posted this question last week but just realized I posted it to the wrong forum. So, Im posting it again here. I am currently using the FlexIO2 module along with eDMA on a few projects. So far it has all worked out very well. Yesterday I noticed this diagram in the document "IMXRT1060RM Rev. 3, 07/2021". It's interesting that FlexIO3 is shown here as tightly coupled with the CPU, while FlexIO modules 1 & 2 are located with the rest of the peripherals. I have not noticed any mention of this difference in chapter 50 on FlexIO.

How is the FlexIO3 module different than FlexIO 1 & 2?

Thanks!

markflamer_0-1654006993915.png

 

0 件の賞賛
返信
1 返信

1,202件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @markflamer ,

Please see Figure 28-1 in RM. The ARM core can access FlexIO3 faster than FlexIO1/2. To access FlexIO1/2, the route is AXI->AIPS->FlexIO1/2. But to access FlexIO3, it is more directly. And AXI speed is 132M maximum, but the AHBP is low-latency and much faster.

 

Regards,

Jinf

0 件の賞賛
返信