First byte of UART data received through DMA is not the right one

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

First byte of UART data received through DMA is not the right one

621件の閲覧回数
hanmant
Contributor III

Hello.

I am using the RT1020 processor.

In my test , I am sending 32 bytes message ,these message i receive using DMA uart .When I look at the data received, the last byte is at the first place, always. There is never any other or additional shift.

I can understand it is byte remaining from the previous comm and missed out from the previous reading but why is it so stable (always one byte and always the correct one).

Correct byte sent

22, 0, 0, 0,14, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, F,54,26,4E,

but I received bytes

4E,22, 0, 0, 0,14, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, F,54,26,

why it is happening .

Below is initialization of DMA uart

#if defined(FSL_FEATURE_SOC_DMAMUX_COUNT) && FSL_FEATURE_SOC_DMAMUX_COUNT

/* Init DMAMUX */

DMAMUX_Init(EXAMPLE_LPUART_DMAMUX_BASEADDR);

/* Set channel for LPUART */

DMAMUX_SetSource(EXAMPLE_LPUART_DMAMUX_BASEADDR, LPUART_TX_DMA_CHANNEL, LPUART_TX_DMA_REQUEST);

DMAMUX_EnableChannel(EXAMPLE_LPUART_DMAMUX_BASEADDR, LPUART_TX_DMA_CHANNEL);

 

DMAMUX_SetSource(EXAMPLE_LPUART_DMAMUX_BASEADDR, LPUART_RX_DMA_CHANNEL, LPUART_RX_DMA_REQUEST);

DMAMUX_EnableChannel(EXAMPLE_LPUART_DMAMUX_BASEADDR, LPUART_RX_DMA_CHANNEL);

#endif

 

/* Init the EDMA module */

//EDMA_GetDefaultConfig(&DMA0_config);

EDMA_Init(EXAMPLE_LPUART_DMA_BASEADDR, &DMA0_config);

 

LPUART_GetDefaultConfig(&lpuartConfig);

lpuartConfig.baudRate_Bps = UART3_BAUDRATE;

lpuartConfig.enableTx = true;

lpuartConfig.enableRx = true;

 

LPUART_Init(DEMO_LPUART, &lpuartConfig, DEMO_LPUART_CLK_FREQ);

EDMA_CreateHandle(&g_lpuartTxEdmaHandle, EXAMPLE_LPUART_DMA_BASEADDR, LPUART_TX_DMA_CHANNEL);

EDMA_CreateHandle(&g_lpuartRxEdmaHandle, EXAMPLE_LPUART_DMA_BASEADDR, LPUART_RX_DMA_CHANNEL);

 

/* Create LPUART DMA handle. */

LPUART_TransferCreateHandleEDMA(DEMO_LPUART, &g_lpuartEdmaHandle, LPUART_UserCallback, NULL, &g_lpuartTxEdmaHandle,

&g_lpuartRxEdmaHandle);

/* Channel CH0 initialization */

/* Set the DMA 0 channel priority */

// EDMA_SetChannelPreemptionConfig(EXAMPLE_LPUART_DMA_BASEADDR, DMA0_CH0_DMA_CHANNEL, &DMA0_CH0_preemption_config);

// /* Channel CH1 initialization */

// /* Set the DMA 1 channel priority */

// EDMA_SetChannelPreemptionConfig(EXAMPLE_LPUART_DMA_BASEADDR, DMA0_CH1_DMA_CHANNEL, &DMA0_CH1_preemption_config);

 

 

 

/* Interrupt vector DMA0_DMA16_IRQn priority settings in the NVIC. */

NVIC_SetPriority(DMA0_DMA_CH_INT_DONE_0_IRQN, DMA0_DMA_CH_INT_DONE_0_IRQ_PRIORITY);

 

/* Interrupt vector DMA0_DMA17_IRQn priority settings in the NVIC. */

NVIC_SetPriority(DMA0_DMA_CH_INT_DONE_1_IRQN, DMA0_DMA_CH_INT_DONE_1_IRQ_PRIORITY);

タグ(3)
0 件の賞賛
返信
3 返答(返信)

560件の閲覧回数
hanmant
Contributor III

Hi @Sam_Gao 

0 件の賞賛
返信

539件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @hanmant,
Sorry for the delayed response. Using the SDK (version 25.03) example called "lpuart_edma_transfer," I modified the macro named ECHO_BUFFER_LENGTH to 32, and it is working correctly. Please ensure that your DMA is properly configured, especially the function called LPUART_SendEDMA. It is likely that the number of major loops is set lower than the buffer size.
BR
Habib

0 件の賞賛
返信

561件の閲覧回数
hanmant
Contributor III

Hi @all,

waiting for response

0 件の賞賛
返信