Fault on backlight circuit of MIMXRT1050-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fault on backlight circuit of MIMXRT1050-EVK

1,530 Views
abertu
Contributor II

I have done some climatic test using the dev-board MIMXRT1050-EVK.
After few hours I have stopped because I my TFT was off.
I have found U8 (UM1661) hot and C88 (4.7 uH, 6.3 V) in shortcircuit.
The rated voltage of the capacitor is not enough to be used for the backlight circuit, it's required at least a 25 V.

Tags (2)
0 Kudos
Reply
1 Reply

1,365 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Angelo,

thank you for your input. I will report it to the appropriate team so they can examine this case.

Reards,

Carlos

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----