Failed to to run camera example project on RT1170 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failed to to run camera example project on RT1170 EVK

Jump to solution
1,504 Views
samuelzhang
Contributor III

I failed to run "tensorflow_lite_micro_label_image_cm7" example on my RT1170 EVK.

Test environment:

MCUEXPRESSO: V11.6.1
SDK RT1170-EVK: V2.12.1
CAMERA: R5640AA

samuelzhang_0-1666234319062.png

samuelzhang_1-1666234407752.png

 

Then I observed that camera initialization failed via console.

samuelzhang_2-1666234467559.png

 

I investigated into source code and found the error caused by:

samuelzhang_3-1666234564190.png

So I need your help to verfify this example project on your side on the same board - RT1170 EVK with the same camera.

If it desen't fail in your side, please tell me how you make this.

Otherwise, please help modify this example project to make it run smoothly.

 

 

0 Kudos
Reply
1 Solution
1,466 Views
samuelzhang
Contributor III

I've asked NXP FAE to run the same test on the EVK board in NXP LAB.

Thanks so much.

View solution in original post

0 Kudos
Reply
5 Replies
1,269 Views
Mc2023
Contributor IV

Hi @samuelzhang,

Could you tell me from where you bought this camera?

Best regards

0 Kudos
Reply
1,280 Views
RogerY
Contributor I

I have the same issue on RT1170 board. how did you fix it?

0 Kudos
Reply
1,483 Views
samuelzhang
Contributor III

Thanks for your quick reply.

I tried other example projects, but nothing was displayed on screen.

Maybe I should get another EVK board to retry.

 

0 Kudos
Reply
1,485 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @samuelzhang ,

My SDK version is 2.11. It works fine. But I think this is not the version problem. Have you tried other camera demos? Can they work?

There is a readme in the project. Have you read this guide?

Regards,

Jing

0 Kudos
Reply
1,467 Views
samuelzhang
Contributor III

I've asked NXP FAE to run the same test on the EVK board in NXP LAB.

Thanks so much.

0 Kudos
Reply