Fail Debug/Program with MCUxpresso and EVK-MIMXRT1020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fail Debug/Program with MCUxpresso and EVK-MIMXRT1020

跳至解决方案
6,125 次查看
luishs
Senior Contributor I

Hello.

I start working with the EVK-MIMXRT1020, I follow all the instructions on the website, I install MCUXpresso, download and install SDK, install USB driver, open Hello_World source code example, Press Build and Debug to program, but it fails. Attached screenshot of MCUXpresso.


I have also reinstalled Java, but it always fails. I also have an evaluation board for the RT1050, and the problem is the same, none can program and run the program, following the instructions on the RT website.


https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...

Best Regards

RT1020_001.jpg

RT1020_002.jpg

RT1020_003.jpg

标签 (1)
标记 (3)
1 解答
4,749 次查看
luishs
Senior Contributor I

Problem totally solved, and now everything works perfectly. The solution was to simply remove the installation and the directory, and install again but in a NEW directory (in my before tests I always reinstalled in same directory name by default). Therefore, when it is executed from a new directory, the firewall warns about each new process and requests whether to accept the process to grant or not permissions.

Then, after running from a new directory and accepting all the warnings from the firewall, everything works perfectly, Jlink, Multilink and DAP-CMSIS via USB in both versions of MCUXpresso 10.1 and 10.2.

The only thing I did not like, is that NXP at no time they offered help on this problem, not a single suggestion about the problem of a FIREWALL server, and when I knew that the problem came from the firewall they did not give me a solution either to definitely solve the problem.

Thanks to Erich from "MCU on Eclipse" blog, without his suggestion about the firewall, I would not have been able to solve this problem.

These are all messages from the firewall when MCUXpresso is running from a new installation and a new directory, for first time. I accept all the warnings, and in this way, the firewall grants permissions to all the MCUXpresso processes, and everything finally works fine.

ScreenHunter_235.jpg

ScreenHunter_237.jpg

ScreenHunter_236.jpg

ScreenHunter_238.jpg

ScreenHunter_239.jpg

ScreenHunter_240.jpg

ScreenHunter_241.jpg

在原帖中查看解决方案

12 回复数
4,750 次查看
luishs
Senior Contributor I

Problem totally solved, and now everything works perfectly. The solution was to simply remove the installation and the directory, and install again but in a NEW directory (in my before tests I always reinstalled in same directory name by default). Therefore, when it is executed from a new directory, the firewall warns about each new process and requests whether to accept the process to grant or not permissions.

Then, after running from a new directory and accepting all the warnings from the firewall, everything works perfectly, Jlink, Multilink and DAP-CMSIS via USB in both versions of MCUXpresso 10.1 and 10.2.

The only thing I did not like, is that NXP at no time they offered help on this problem, not a single suggestion about the problem of a FIREWALL server, and when I knew that the problem came from the firewall they did not give me a solution either to definitely solve the problem.

Thanks to Erich from "MCU on Eclipse" blog, without his suggestion about the firewall, I would not have been able to solve this problem.

These are all messages from the firewall when MCUXpresso is running from a new installation and a new directory, for first time. I accept all the warnings, and in this way, the firewall grants permissions to all the MCUXpresso processes, and everything finally works fine.

ScreenHunter_235.jpg

ScreenHunter_237.jpg

ScreenHunter_236.jpg

ScreenHunter_238.jpg

ScreenHunter_239.jpg

ScreenHunter_240.jpg

ScreenHunter_241.jpg

4,749 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Luis,

I am pleased that you have made progress and are able to debug with MCUXpresso IDE version 10.2.

MCUXpresso IDE assumes it has localhost telnet access and will request the access it needs from the Windows firewall mechanism. If you make use of a third party firewall, then you will need to manage these requirements.

One thing to point out... if you have multiple installations of MCUXpresso IDE, then each installations copy of LinkServer (Redlinkserv) must have the required firewall access. Our only explanation for the difference in behaviours of versions 10.1 and 10.2 is that at some time in the past, LinkServer from the 10.1 installation had been given the required firewall access.

Yours,

MCUXpresso IDE Support

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

Both versions of MCUXpresso have the same firewall permissions, so that's not the problem. I think I'll have to solve everything by myself, you never made a single suggestion about the firewall, nor now any useful suggestions on how to solve the final problems with errors in version 10.2 using DAP-CMSIS and the Multilink programmer.

This publication will only be useful to prevent other users from losing their time also solving the same problem, but there is practically no support or solutions to the problem from you, on the contrary, I have solved the problem and I have given solution to the community.

You should know perfectly well that practically everyone installs a firewall on their computer, so this problem will be common in most people. But you seem to have never checked something so basic and never notice about it in user manuals or technical documents. And when someone claims you also totally ignore the firewall problems to work with MCUXpresso.

I am surprised in that respect, that a company like NXP of such a poor support, ignoring such basic things, and even more surprised that even then, now you do not give a final solution, about some problems that still persist.

I said, in the end I'll have to solve everything myself. From NXP I have not received the slightest support on this problem.

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

More tests, this with the Multilink PE programmer, fail with MCUXpresso 10.2 if I do not disable the firewall, work well if I disable the firewall. With MCUXpresso 10.1 it works well with or without the firewall enabled.

SEGGER Jlink programmer is currently working perfectly with MCUXpresso 10.1 and 10.2, after giving firewall permissions to Redlinkserv process.  DAP-CMSIS by USB, works perfectly with MCUXpresso 10.1 and gives some errors in MCUXpresso 10.2 if the firewall is enabled, although if I  press OK to the two errors it gives, it seems to work.

In summary, all the current problems have some relation with the firewall and the ports, but only with MCUXpresso 10.2,  no problems with MCUXpresso 10.1.

ScreenHunter_233.jpg

4,749 次查看
luishs
Senior Contributor I

It's strange, now with MCUXpresso 10.1, it does not give any errors and everything works fine. I only get that error from port 3331 with MCUXpresso 10.2, although if I press OK on both errors, it continues and it works. Anyway I would like to eliminate that error.

to bind to port ‘3331’ – No such file or directory (rc 2)
problem connecting to ‘:telnet:3331’
to bind to port ‘3331’ – No such file or directory (rc 2)
problem connecting to ‘:telnet:3331’
to bind to port ‘3331’ – No such file or directory (rc 2)
problem connecting to ‘:telnet:3331’ “

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

Finally, I think I solved the problem with DAP-CMSIS using a USB driver, although only partially. Erich from the blog "MCU in Eclipse" suggested me to disable the firewall, and indeed, that was the problem, the firewall.

I disabled it and it started to work, but if I activated it again, I lost access again. Then I opened the firewall and gave access permission to "Redlinkserv" as seen in the screenshot attached. In this way it starts, but it gives me two errors, although if I press the OK button on both, it continues and starts without problems.


The question now is how to avoid receiving those error messages, it is something of the firewall, because if I disable it, everything works fine, and if I activate it, although I have already given permission "Redlinkserv", I get those errors that seem related to the port 3331 of the firewall.

ScreenHunter_215.jpg

ScreenHunter_213.jpg

ScreenHunter_214.jpg

ScreenHunter_221.jpg

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

Today I have done more tests and it seems that something has advanced. I already did a completely new installation, deleting the MCUXpresso and the SDK, to install them again, and the failures remained the same, this did not solve anything.

What I saw, is that there are two icons of Debug, one with a violet cockroach, and another with a green cockroach. With the second, I can choose the interface that will be used to make Debug, I get options for CMSIS-DAP, Jlink and Multilink. Over here I have finally been able to start the Debug using Jlink or Multilink in MCUXpresso 10.2. If I use the icon of the violet cockroach, it does not work, a screen appears in which it seems that it is permanently looking for the USB CMSIS-DAP interface, which never finds it.

In summary, Debug definitely does not work for me using CMSIS-DAP via USB, in none of the two versions of MCUXpresso, 10.1 and 10.2, it does not find this interface via USB. I have seen the MCU on Eclipse blog, with the tests on the RT1050 evaluation board, and the only difference I have found is that Erich is using Windows 10, and I use Windows7.

Screenshot, using the icon (green cockroach) that gives the option to choose which interface to use to Debug. With this option, I have finally been able to debug with MCUXpresso 10.2 using the Jlink or Multilink programmers, but it fails if I try to use CMSIS-DAP via USB.

ScreenHunter_208.jpg

Screenshot, about what I see if I try to debug using CMSIS-DAP via USB, or by clicking on the violet cockroach icon. MCUXpresso remains locked on this screen, it seems that it is looking for a USB device but never finds it. The same happens with MCUXpresso 10.1. I work with Windows 7 64 bits, maybe this is the problem, because I see in the blog "MCU on Eclipse" that they try it with Windows 10. May be the USB drivers you provide are not compatible with Windows 7 64 bit, or something is wrong to work with this OS version using CMSIS-DAP by USB, or the firmware version of OpenSDA on my boards is wrong or outdated and is not compatible with current USB drivers.

ScreenHunter_201.jpg

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

All that I already did and it continues to fail exactly the same, and only works with the programmers and MCUXpresso version that I have indicated.

1.- OS ---> Windows 7 64 bit.

2 .-How the built in debug probe of your RT board appears to your OS in Device and Printers (or similar).

Here you can see Jlink, Multilink and mbed drivers when connect RT1050 by USB

ScreenHunter_180.jpg

This in Devices and Printers.

ScreenHunter_188.jpg

ScreenHunter_189.jpg

3.- Details of any dialogs you see.

Check my before messages, I have post capture screens of all error messages that show MCUXpresso in 10.1 and 10.2 versions. 

4.- The text content from the Debug Log in the console view. Details of how to get this can be found in section 18.8, "The Console View" of the MCUXpresso IDE v10.2 User Guide.

  4.1.-
  With MCUXpresso 10.1, RT1050 board by USB (DAP LINK CMSIS-DAP Driver)

ScreenHunter_181.jpg

ScreenHunter_184.jpg

ScreenHunter_185.jpg

ScreenHunter_186.jpg

ScreenHunter_187.jpg

4.2.- With MCUXpresso 10.2, RT1050 and RT1020 boards.
Tested with Jlink, Multilink and USB (DAP LINK CMSIS-DAP driver). There is no option to choose a different console mode because MCUXpresso remains locked looking for programmers or USB card, and never finds anything, finally I must cancel. With MCUXpresso 10.2 everything fails, Jlink; Multilink and USB (DAP LINK CMSIS-DAP driver), impossible to do anything with this version of MCUXpresso.


ScreenHunter_182.jpg

ScreenHunter_173.jpg

.

0 项奖励
回复
4,749 次查看
art
NXP Employee
NXP Employee

Try to forcedly run the MCUXpresso IDE software in Administrator mode.

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

Just now testing again with RT1050 by USB CMSIS-DAP.

With MCUXpresso 10.2, the software seems to be looking for drivers or programmers, it never finds anything, and I have to cancel it.

ScreenHunter_173.jpg

And with MCUXpresso 10.1, at least it finds the USB CMSIS-DAP drivers, but it ends up giving error.

ScreenHunter_174.jpg

ScreenHunter_176.jpg

ScreenHunter_177.jpg

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

Its working in Administrator mode, and fail. Today I have check my RT1020 and RT1050 boards, with MCUxpresso 10.1 and 10.2, programmers Jlink and Multilink, also tested by USB with DAP LINK CMSIS-DAP Driver.


Only works RT1050 + Jlink or Multilink PE  + MCUXpresso 10.1, and RT1020 + Jlink  + MCUXpresso 10.1

RT1050 + MCUxpresso 10.1.0 + DAP LINK CMSIS-DAP Driver --> FAIL
RT1050 + MCUxpresso 10.2.0 + DAP LINK CMSIS-DAP Driver --> FAIL
RT1020 + MCUxpresso 10.1.0 + DAP LINK CMSIS-DAP Driver --> FAIL
RT1020 + MCUxpresso 10.2.0 + DAP LINK CMSIS-DAP Driver --> FAIL

RT1050 + MCUxpresso 10.1.0 + Multilink PE programmer --> OK
RT1050 + MCUxpresso 10.2.0 + Multilink PE programmer --> FAIL
RT1020 + MCUxpresso 10.1.0 + Multilink PE programmer --> FAIL
RT1020 + MCUxpresso 10.2.0 + Multilink PE programmer --> FAIL

RT1050 + MCUxpresso 10.1.0 + Jlink programmer --> OK
RT1050 + MCUxpresso 10.2.0 + Jlink programmer --> FAIL
RT1020 + MCUxpresso 10.1.0 + Jlink programmer --> OK
RT1020 + MCUxpresso 10.2.0 + Jlink programmer --> FAIL

ScreenHunter_167.jpg

ScreenHunter_168.jpg

ScreenHunter_170.jpg

ScreenHunter_171.jpg

0 项奖励
回复
4,749 次查看
luishs
Senior Contributor I

I have install now MCUxpresso 10.1.0, and this recognize the DAP Link CMSIS DAP driver, Program, Run and Debug.

But fail with MCUxpresso 10.2.0. What happen, what is the problem with MCUxpresso 10.2.0 ??

ScreenHunter_125.jpg

0 项奖励
回复