FT5336 driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FT5336 driver

1,207 Views
nxpuserme
Contributor I

I use a RK043FN02H-CT LCD panel to working with the MIMXRT1060-EVK, now I need a FT5336 touch IC driver, please send me if anyone has it. Thanks very much.

Tags (1)
0 Kudos
Reply
1 Reply

1,204 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
There's the datasheet of FT5336 and the attachment is the driver of FT5406, please use it as a template and adapt it by referring to the above datasheet.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply