1.Any API to do operation on internal flash in IMXRT1064?
1.Please suggest me the approach to do FOTA update using Ethernet (application program to download the firmware into external flash hyperflash/ QSPI NOR flash ) in imxRT1064 board.?
2.Amazon FreeRTOS OTA demo code is supported for imxRT1060 but not given SDK Amazon FreeRTOS OTA demo code for imxRT1064 ,is it available for IMXRT1064 board?
3. Any suggestion using secondary bootloader to do FOTA?
This is a duplicated thread. Please refer to this post: https://community.nxp.com/thread/522713