FILT of Quadrature Decoder (QDC) cannot be set

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FILT of Quadrature Decoder (QDC) cannot be set

跳至解决方案
574 次查看
Shuhei_D
Contributor I

Hello,

I want to set QDC FILT with i.MXRT1170, but even if I set 0xffff to FILT as shown below, I can only set up to 0x7ff.

code.PNG

register.PNG

How to set PRSC of FILT?

0 项奖励
回复
1 解答
492 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi again @Shuhei_D,

We have confirmed that this is a documentation error. PRSC does not exist in the FILT register on RT1170. The next release of the RM and the SDK will be corrected from this mistake.

Thanks for reporting this issue,
Edwin.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
493 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi again @Shuhei_D,

We have confirmed that this is a documentation error. PRSC does not exist in the FILT register on RT1170. The next release of the RM and the SDK will be corrected from this mistake.

Thanks for reporting this issue,
Edwin.

0 项奖励
回复
544 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Shuhei_D,

I was able to replicate this problem on my side. It could be a bug on the Peripherals+ side, on the SDK side, or even an errata on the chip. I will investigate further and come back once I have an answer.

BR,
Edwin.