[FATAL ERROR] Import the App Software Pack Into MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[FATAL ERROR] Import the App Software Pack Into MCUXpresso IDE

Jump to solution
789 Views
sukhwan
Contributor III

 

I have a fatal error in STEP 4.1 Option #1: Get the App Software Pack with MCUXpresso IDE at https://github.com/nxp-appcodehub/ap-dvs-pvt-sensor/blob/mcux_release_github/dvs_pvt_sensor/app/evkm...

 

This issue looks a similar issue that I reported at https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/can-t-download-mcu-examples-from-github/m-p/2138...

 

==================STEP 4.1 Option command log======================

$west update
=== updating mcux-sdk (core):
--- mcux-sdk: initializing
Initialized empty Git repository in ~/nxp-githubs/appswpacks_dvs_pvt_sensor/core/.git/
--- mcux-sdk: fetching, need revision MCUX_2.11.0
remote: Enumerating objects: 80743, done.
remote: Counting objects: 100% (7353/7353), done.
remote: Compressing objects: 100% (917/917), done.
error: RPC failed; curl 92 HTTP/2 stream 0 was not closed cleanly: CANCEL (err
error: 6264 bytes of body are still expected
fetch-pack: unexpected disconnect while reading sideband packet
fatal: early EOF
fatal: fetch-pack: invalid index-pack output
FATAL ERROR: command exited with status 128: fetch -f --tags -- https://github.com/nxp-mcuxpresso/mcux-sdk MCUX_2.11.0

0 Kudos
Reply
1 Solution
691 Views
sukhwan
Contributor III

Now it works after I reported it to our company IT.

Thanks.

View solution in original post

0 Kudos
Reply
5 Replies
692 Views
sukhwan
Contributor III

Now it works after I reported it to our company IT.

Thanks.

0 Kudos
Reply
782 Views
sukhwan
Contributor III

===========Step 4.2 Option 2 log=================
Failed to execute command
Cloning into '~/nxp/appswpacks-dvs-pvt-sensor/.west/manifest-tmp'...
error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.
error: 3468 bytes of body are still expected
fetch-pack: unexpected disconnect while reading sideband packet
fatal: early EOF
fatal: fetch-pack: invalid index-pack output
FATAL ERROR: command exited with status 128: git clone --branch mcux_release_github https://github.com/NXPmicro/appswpacks-dvs-pvt-sensor ~/nxp/appswpacks-dvs-pvt-sensor/.west/manifest-tmp

0 Kudos
Reply
785 Views
sukhwan
Contributor III

Step 4.2 Option 2 also has the same fatal error.

0 Kudos
Reply
739 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @sukhwan ,

 

I just tried with the option 2, but looks like it works well as expected. Please kindly refer to the following for details.

Kan_Li_0-1753683795617.png

The command I tried on my side:

Kan_Li_1-1753683829374.png

 

Was there any network issue from your side?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply
740 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @sukhwan ,

 

May I have your MCUXpresso IDE version? 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply