Hello experts,
I'm new to SD card boot for RT1050, I find an application note AN12107, it shows the steps about boot from SD
card using SDK demo.
I thought the application image should download into SD card, after boot, copy it to ITCM to run.
While in the guide and code , I haven't find address related to SD card, only ITCM and DTCM space:
Could you please explain the theory of it .
Any suggestion will be appreciate.
BR
fan
Hi fan
one can look at boot flow described in Figure 8-6. Expansion device boot flow
i.MX RT1050 Processor Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf
Memories addresses in Table 1 AN12107, Figure 1 and Table 5
explaining boot process.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello igor,
Thanks for your comment.
While I have read boot process you mentioned, I just want to know the "address related to SD card, boot".
I don't know why when use SD card boot, place code into ITCM, not in SD address (Also I don't the address ).
Take hyperfalsh boot as an example , we put the code into 0x60000000(the address for Hyperflash) ,what about
SD Card boot.
Thanks a lot!
BR
fan
Hi igor,
I check the BD file imx-itcm-unsigned.bd (AN12107 mentioned) "imx-itcm-unsigned.bd" ,
the IVT address is 0x1400, the entry is 0x2000, they are all ITCM address.
So I was wondering what relationship with SD card.
BR
fan
Hi fan
actually this BD file does not have relation to read boot process,
this relates to *.bd files description, as these files are used elftosb utility.
These bd files are not intuitively understandable, so one can check elftosb documentation.
Suggest to check flashloader documentation.
Programmers (Flash, etc.) (1)
Flashloader i.MX-RT1050
i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP
Elftosb Guide
https://www.nxp.com/docs/en/user-guide/KBLELFTOSBUG.pdf
Best regards
igor