Hi,
i want to use one MII-Ethernet and the SWD for debugging.
Is it correct, that i have to use the Ethernet2 because SWD and MII0 share the same pins?
thanks,
Thomas
Solved! Go to Solution.
Hi,
Thanks for your reply and clarification.
1) Is it correct, that SWD works with RMII-Interface on ENET or (R)MII-Interface on ENET2 but not with MII-Interface on ENET?
-- Yes, if you need to use debug tool to connect the SWD interface for debugging.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
for the RT1064 i found this pinout for SWD and ENET:
| Instance | Port | Pad |
| SWD | SWD_DIO | GPIO_AD_B0_06 |
| SWD_CLK | GPIO_AD_B0_07 | |
| ENET | ENET_RX_CLK | GPIO_AD_B0_06 |
| ENET_TX_ER | GPIO_AD_B0_07 |
ENET_RX_CLK and ENET_TX_ER are used by a full MII-Interface PHY (e.g. KSZ8863MLL).
Is it correct, that SWD works with RMII-Interface on ENET or (R)MII-Interface on ENET2 but not with MII-Interface on ENET?
Thanks
Thomas
Hi,
Thanks for your reply and clarification.
1) Is it correct, that SWD works with RMII-Interface on ENET or (R)MII-Interface on ENET2 but not with MII-Interface on ENET?
-- Yes, if you need to use debug tool to connect the SWD interface for debugging.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I was wondering if you can describe your question or finding in detail.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------