Hi Diego,
thanks for your response, but I had already taken care of these issues previously, so it did not help.
Anyway, I have changed tacks now: instead of trying to use the pre-built image, I am now trying to build and run the ecat/digital_io example from SDK, using the AN14155 User Guide (Using the i.MX RT1180 EtherCAT together with BECKOFF TwinCAT3 and SSC tool Rev. 1.0)
Here also I am facing the same problem. I am able to build, flash and run the example (both for CM33 and CM7). I have put a printf in the main loop in digitial_ip.c to verify that it is indeed running.
However, I am stuck in section 5.1.8 of AN14155 : If I do a scan for EtherCAT devices using TwinCAT, it says "No I/O Devices found". I have tried connecting the Ethernet cable to both J28 and J32.
I have made the following jumper settings: J63, J73 and J72,J65 have been moved to 1-2 shorted position (non default position)
I don't know if any other jumper settings or other HW settings are required for Ecat. Other than these , all jumpers are in the default position (what it was out of the box). The only other jumper change I made was for using the Segger probe (JP5 shorted).
Btw, I have also tried running the ICE Tool. Same situation as before.
I would appreciate if you could provide any inputs
thanks
regards
Pnc