Error in MI Command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in MI Command

2,929 Views
dhanushkumar_n
Contributor I

Hi,

i am using IM.XRT1020-EVK for development i was using this since month but it is throwing error saying unable to execute MI command since past 2 days ,Can anybody let me know what could be the reason for this error ,below i have attached the screen shots ,please guide me solving this issue .

Labels (1)
0 Kudos
Reply
2 Replies

2,877 Views
dhanushkumar_n
Contributor I

Thank you .

0 Kudos
Reply

2,878 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Dhanush KumarN ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you. 
To provide the fastest possible support, I'd highly recommend you to refer to the post:
https://community.nxp.com/thread/480595 for details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----