Errata ERR050577, SDRAM Burst Length

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Errata ERR050577, SDRAM Burst Length

Jump to solution
2,198 Views
jaredm
Contributor III

Hi, I am looking for additional details on Errata ERR050577. I am working on the RT1052. If I follow the recommendation of the Errata, the burst length is configured as 1 and there will be significant SDRAM performance reduction.

Is there a different workaround for this Errata that allows burst length > 1? What if SDRAM3[UT] (Refresh urgent threshold) and/or STDRAM[RT] (Refresh timer period) values are reduced?

Thanks in advance.

 

0 Kudos
Reply
1 Solution
2,156 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Jared,

Unfortunately, there are no specific regulations to avoid this errata. The only requirement to avoid the errata effect is to set the burst length to 1.

Best regards,

Felipe

View solution in original post

3 Replies
2,180 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Jared,

Unfortunately, there is no other workaround documented that can allow you to use burst length > 1. Sorry for the inconvenience.

Best regards,

Felipe

0 Kudos
Reply
2,177 Views
jaredm
Contributor III

Hi Felipe,

Is there a way to determine whether the error condition can occur? Or common problem cases? For example, large DMA transfers?

The reason I ask is because my application may avoid the error condition. I am not using DMA. My application does image processing on 5MP images, so the CPU is moving large amounts of data in/out of SDRAM. If burst=1, it may decrease performance significantly.
 
Thanks,
jaredm
 
0 Kudos
Reply
2,157 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Jared,

Unfortunately, there are no specific regulations to avoid this errata. The only requirement to avoid the errata effect is to set the burst length to 1.

Best regards,

Felipe