Encrypted Image on RT1020 - how is it done please?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypted Image on RT1020 - how is it done please?

1,647 Views
rshipman
Senior Contributor I

Hi,

I am trying to encrypt, download and run an image for the RT1020 eval board.

I've have tried to follow the document AN12079.pdf.

I've been given the RT1020 release package (which has the flashloader and .bd files).

I've found a whole bunch of other documents, relating to security, hab, elftosb, etc.

But I've not managed to get anywhere near getting something ready to download, let alone actually donwload it and see it run.

And I've also tried using the NXP-MCUBootUtility, but did not get anywhere.

Can anyone please give me a tried and tested example of building, encrypting, downloading and running a binary (e.g. iled_blinky) for the RT1021 eval board.

Many thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,556 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and
the opportunity to serve you.
To provide the fastest possible support, I want to point you to a
similar question that has been answered on our NXP community.
Please refer to https://community.nxp.com/thread/519126?commentID=1245513#comment-1245513 
to view the details.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,556 Views
t_thurgood
Contributor III

I am trying to do this with our project. I have been able to produce encrypted images and SRKs, but having problems downloading.

You can see this thread for more info...

https://community.nxp.com/message/1245513?commentID=1245513#comment-1245513 

0 Kudos
Reply