Empty frame received (RT1176)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Empty frame received (RT1176)

188 次查看
luk1
Contributor I

Ethernet receives data for a period of time and then fails to receive new data.The " ENET_GetRxFrameSize "show that the length of the received frame is 0. The ' control ' element of the ' curBuffDescrip ' always comes as 0x8000 and as a result ' kStatus_ENET_RxFrameEmpty ' is returned.At this time, if the network driver is re-initialized, data reception can return to normal. What could be the reason for this situation?

My board is based on the RT1176 development, using the SDK 2.11.

0 项奖励
回复
1 回复

141 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @luk1,

Thank you for getting in touch, I apologize for the delay

To narrow down the issue, could you please help me test with the latest version of SDK v15.1, select an example closer to your application, and share the results with me?

Please inform me if you have any additional information about your application or if you discover anything new during this time

0 项奖励
回复