Edgefast bluetooth not working with Android 14 using AVRCP fragmented messages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Edgefast bluetooth not working with Android 14 using AVRCP fragmented messages

977 Views
danix2k-dxc
Contributor II

Hello everyone,

I'm using an i.MXRT1170-EVK (not B version) and I'm trying to connect my phone to the board. I modified the HW for the BT external micro (I'm using a 1ZM Murata M2 chip) and I'm trying to retrieve GET ELEMENT Attribute from my phone using evkmimxrt1170_edgefast_bluetooth_shell. Here we are talking about AVRCP profile to retrive media information from the phone.

It seems that Edgefast BT dosen't handled fragmented packet sent by Android 14; the example goes into an ASSERT following the steps below:

  1. bt.init
  2. br.connect <phone MAC addr> //Connect to an Android 14 phone - mine is a Samsung A53
  3. avrcp.init_ct
  4. avrcp.ctl_connect (before performing this step, make sure BR is still connected)
  5. avrcp.ct_test_case 18 // to retrive getAttribute Element

At this point we go through an ASSERT because Android 14 sends a fragmented message but Edgefast BT try to parse this message as if it were completed and we have the assert in net buf API (byte missing).

Can someone check this behavior and tell me if an Edgefast BT version is expected to fix this behavior with the newest Android version? OR can someone tell me if we can use a more reliable BT stack implementation for NXP rt1170 board - also if you have to pay for it?

 

Thanks.

 

0 Kudos
Reply
6 Replies

932 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Thank you for the information. I am checking this situation. Please give me some time to handle this.

 

As soon as I have something to share, I will let you know.

 

Regards,

Ricardo

887 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Could you please help me confirm your WiFi device?

 

Regards,

Ricardo

0 Kudos
Reply

865 Views
danix2k-dxc
Contributor II

Hello,

I'm using a Murata 1ZM M2 module; only the BT part (I previously wrote the wrong module on the main post).

I confirm a Murata 1ZM M2 module

 

Regards

0 Kudos
Reply

603 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

I really apologize for a late reply. We have been checking you issue.

 

Could you please helps us checking if this behavior is happening on another Android14 devices? (Other than the Samsung A53).

 

Regards,

Ricardo

0 Kudos
Reply

555 Views
danix2k-dxc
Contributor II

Hello,

I tested it with another Samsung phone (S21) and with a Pixel 7 Pro.

With Pixel 7 Pro it works if the track name or the track album is shorter than 22-24 byte because it doesn't send fragmented packet.

Instead Samsung sends always a fragmented packet even if the track name or the track album is shorter.

Regards.

0 Kudos
Reply

426 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

I sent you a private message.

 

Regards,

Ricardo

0 Kudos
Reply