Does the USBOTG1 interface of IMXRT1170-EVK support the UVC protocol?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does the USBOTG1 interface of IMXRT1170-EVK support the UVC protocol?

1,345件の閲覧回数
TheSix
Contributor I

Does the USBOTG1 interface of IMXRT1170-EVK support the UVC protocol?Do I need to install a UVC driver to transmit video data using the UVC protocol on the USBOTG1 interface?

0 件の賞賛
返信
2 返答(返信)

1,308件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @TheSix,

It seems that in fact IMXRT1170 supports UVC protocol.

There is an application note for the IMXRT1050 that might be useful for you: Developing a simple UVC device based on i.MX RT1050.

Also, there is a community thread of a client that uses UVC protocol with an IMXRT1170: iMXRT1176 MIPI-CSI2 to UVC reducing the frame buff... - NXP Community.

Best regards, Raul.

1,290件の閲覧回数
TheSix
Contributor I

OK,thanks you .This is useful.

0 件の賞賛
返信